Whether you are looking at purchasing a new freeze dryer or already have a freeze dryer, Labconco has articles that will help you make the best choices for your laboratory. We also offer articles on the freeze dry process if you are unfamiliar with it.
Unsure of the best way to process your samples? These articles will help understand the benefits of lyophilization and what is required.
If you are in the beginning stages of purchasing a lyophilizer and are not sure what freeze dryer to choose, here are some articles that will help:
Applications for the freeze dry process are extensive, almost anything can be freeze dried, but some samples turn out different from others. You may get a nice cake, a dry powder, or a gummy sample at the end of the process.
Read through these articles for applications currently being done and helpful hints for the freeze dry process.
Do you already have a freeze dryer and want to optimize your process? If so, the articles below will help.
Once you’ve run the freeze dryer, the following articles will help you maintain the unit for years to come.
chevron_left | How Heater Size Affects Glassware Washer Run Times | Articles | Fume Hood Resources: We’ve got you covered! | chevron_right |