A new patent has been issued to Labconco for the Type C1 biosafety cabinet that changed the way life science laboratories are designed. The first biosafety cabinet with a versatile exhaust system was an R&D 100 Award for Innovation Finalist when it was first released to the market, and has had a growing presence in new lab designs ever since.
The video below explains the advancements in Labconco's newest, most innovative biosafety cabinet, the Purifier Axiom Class II, Type C1.
The Axiom is the only BSC that allows you to switch between type A mode and type B mode, due to its Omni-Flex™ design. The 3-piece Chem-Zone™ work surface makes chemical handling safer and easier in Type B mode, and Active Protection Protocol™ sets this BSC apart as the safest ducted cabinet yet created.
chevron_left | Introduction to freeze drying | Articles | How to select the right fume hood sash glass (video comparison) | chevron_right |