Lyophilization is a dehydration method that involves the removal of solvent from a frozen sample under vacuum, resulting in a porous structure with preserved physical and chemical properties. This technique is particularly important for the creation of next-generation materials such as hydrogels and aerogels due to its ability to maintain the nanopore structures, stability, and functionality of delicate biomaterials and polymers.
The process consists of three main stages: freezing, primary drying, and secondary drying. During the freezing stage, the sample is cooled to below its freezing point, causing the formation of ice crystals within. In the primary drying stage, the pressure is reduced, and heat is applied to sublimate the ice directly into vapor, bypassing the liquid phase. Finally, in the secondary drying stage, residual moisture is removed through desorption under vacuum, resulting in a dry product. The precise control of temperature, pressure, and time during each stage is critical for achieving optimal results and laboratory-grade lyophilization equipment enables the intricate fine tuning required to create these materials in the most efficient way.
Both hydrogels and aerogels utilize polymers and medium replacement to create a final, usable product. So, what’s the difference between these two emerging materials? Hydrogels are networks of hydrophilic polymers designed to retain large amounts of water, whereas aerogels are polymer networks primarily comprised of air. The creation of each material looks very similar during the lyophilization phase, but each resulting product serves a different function.
Download the complete article to continue reading.
chevron_left | Navigating Glove Box Selection | Articles | Labconco Vacuum Pump Buyer's Guide: Finding the Perfect Pump for Your Needs | chevron_right |